STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Why do I get overrun error when using DCMI?

BACKGROUNDproject purpose: capture a picture every 2 secondsboard: nucleo stm32h743zi2 at 480MHzide: stm32cubeidecamera module: ov7670 at 24MHzCONFIGURATIONThe project was initialized using stm32cubeMX with I2C and DCMI initialized. The ov7670 is con...

YL.11 by Associate II
  • 4101 Views
  • 4 replies
  • 5 kudos

Resolved! Hardfault on STM32F769 using TouchGFX

hi I use touchgfx 4.24 , STM32CubeIDE 1.16 and STM32cubeMX 6.12 I do a project with touchgfx, I import it on cubeide, no problems to launch it on the card (STM32F769I-DISCO) I make a modification ( uart 5) on the file ioc and the bilioteque (newlib r...

pascalous by Associate II
  • 5659 Views
  • 16 replies
  • 1 kudos

Mixed image on screen

Hi,I have a custom board with STM32H743 and working on a project by TouchGFX 4.24. When the device power on or reset, some times I have a mixed image including numbers, pictures and ..., which I attached the image... and some times every thing is Ok ...

MHaji.1 by Senior
  • 7317 Views
  • 13 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.