STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Text Area alignment change

How to change the alignment of textarea from the default style set in touchgfx designer? In touchgfx designer(Version:4.21.3) I have set to Left alignment. I use this textarea for multiple purposes, for few I need to set to Left alignment and for few...

BhavyaSri by Associate III
  • 7000 Views
  • 14 replies
  • 3 kudos

Resolved! Pausing function during keyboard input

Hi I am using the TouchGFX keyboard to input data into fields on a number of settings screens. Since the screens are small, I cannot afford the option of Cancel and Enter buttons as used in the demo. Instead I have added 2 buttons to the keyboard for...

Kenbit by Associate III
  • 9419 Views
  • 24 replies
  • 4 kudos

IAR Project generation issues

Hello,I'm experiencing issues with TouchGFX file/folder generation.Below the steps I've followed and issues encountered:Create and generate CubeMX project (NUCLEO-U545RE-Q) with TouchGFX, ThreadX and SPI for IAROpen touchgfx.part file, add some text ...

George.P by Associate III
  • 2358 Views
  • 4 replies
  • 0 kudos

TouchGFX does not build.

When I install TouchGFX and run the Designer to run the example code, the build fails with an error as shown below.=======================================================================================Compile    make -f ../gcc/Makefile -j10     Read...

STM32H750 discovery not working

Hello, I just bought a STM32H750B-DK and when i tried to flash a sample application from TouchGFX, i got a white screen and the usb programming is not working anymore. I connected via External PowerSupply and STLINK and i can see the board and flash ...

BHure.1 by Associate III
  • 2874 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.