2021-03-12 2:31 AM
I created a basic project on the TouchGFX Designer and wrote a function in my own cpp file using touchgfx library. I want that when the button is clicked ,the function is called to ScreenView.cpp or ScreenViewBase.cpp from my own cpp file and change the color of the box.
This is my cpp file.
#include <touchgfx/Color.hpp>
#include <touchgfx/widgets/Box.hpp>
#include <gui/screen1_screen/Screen1View.hpp>
#include <gui/screen1_screen/Screen1Presenter.hpp>
ChangeColor::ChangeColor()
{
Screen1View::box1;
box1.setColor(touchgfx::Color::getColorFrom24BitRGB(51, 168, 35));
box1.invalidate();
}This is the Screen1View.cpp where I want to call my function.
#include<gui/ChangeColor.hpp>
#include <touchgfx/Color.hpp>
Screen1View::Screen1View():
buttonCallback(this, &Screen1View::buttonCallbackHandler)
{
}
void Screen1View::setupScreen()
{
Screen1ViewBase::setupScreen();
button1.setAction(buttonCallback);
}
void Screen1View::tearDownScreen()
{
Screen1ViewBase::tearDownScreen();
}
void Screen1View::buttonCallbackHandler(const touchgfx::AbstractButton& src)
{
if (&src == &button1)
{
//Interaction1
//When button1 clicked execute C++ code
//Execute C++ code
ChangeColor();
}
}I can't access the box. I think that I need to access the Screen1Presenter. How can I access?
2021-03-12 7:15 AM
Well, there's a few things wrong here:
If you want to make this function in an external cpp file, something like this would probably work.
// changecolor.hpp
#include <touchgfx/widgets/Box.hpp>
class ChangeColor{
public:
static void changeColor(touchgfx::Box& b);
};
// changecolor.cpp
#include "changecolor.hpp"
#include "touchgfx/Color.hpp"
void ChangeColor::changeColor(touchgfx::Box& b){
b.setColor(...);
b.invalidate();
}
// in Screen1View.cpp
if (&src == &button1)
{
ChangeColor::changeColor(box1);
}
2021-03-12 7:39 AM
Also, this seems a bit like an XY problem - why do you want to call code in another file? Why not write it in the Screen1View.cpp file? What are you trying to accomplish?
2021-03-15 6:05 AM
Thank you. It worked.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.