2022-04-07 2:08 AM
Hello all,
I use thousands of widgets in a project, and hundreds widgets in each screen.
Each widget occupies a chunk of static ram memory, it result in a large memory used.
And the ram widget used cannot release when screen changed.
2022-04-07 6:52 AM
Hello V.H,
Wow, thousands of widgets, that's impressive. Are you sure there is no way to reduce that amount ? :smirking_face:
The memory usage in internal RAM thus does not depend on the number of screens in the application, but on the size of the largest screen. So I advise you to try to reduce the size of your largest screen first.
Yes you can use SDRAM to expand ram memory if you need more. You can read this article for more info about it.
/Osman
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.