2021-01-26 10:30 AM
I met a strange "problem" with TGFX. Let's say, on one screen, it contains a few buttons and a container. the container is on top of the screen and invisible when the screen is initialized. The problem is when I set the container visible, I found buttons under the container are touchable, even though I cannot see them (the container covers the whole screen). Is this normal? what should I do if I want only the "visible" widgets being "activated". Thanks in advance.
Solved! Go to Solution.
2021-01-27 7:42 PM
Hello,
I'll see with the team if we should change that in the future.
For now, one way to do it would be to add a ClickListener to your container. You can do this directly in the Designer (see picture below)
When your question is answered, please close this topic by choosing Select as Best.
/Alexandre
2021-01-27 7:42 PM
Hello,
I'll see with the team if we should change that in the future.
For now, one way to do it would be to add a ClickListener to your container. You can do this directly in the Designer (see picture below)
When your question is answered, please close this topic by choosing Select as Best.
/Alexandre
2021-01-28 5:48 AM
Thanks. it solves our problem. we have created a custom modal window to wrap our containers to fix this issue. but your solution is much better than ours. I have selected it as best.
2021-01-29 8:26 AM
I have the same problem with vertical menu. My vertical menu cover a part of the screen (more than half screen) and when it is full expanded allows to interact with all other objects in the screen behind it. I want to try this solution hoping it can solve this "problem". I will write the result as soon as possibile.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.