2020-04-08 7:26 AM
I'm trying to integrate the display in question with TGX 4.13. This is the LCD module.
I developed the drivers for both display and touch, configured the project and trying to follow what is reported in the documentation at this link (spi scenarios for ST7789H2).
I have an error during compilation which is as follows:
../TouchGFX/target/TouchGFXHAL.cpp:91:8: error: 'class TouchGFXHAL' has no member named 'copyFrameBufferBlockToLCD'; did you mean 'setFrameBufferAllocator'?How to solve?
2022-01-03 11:12 PM
Thanks Martin,
I think your proposed approach is indeed more efficient than just waiting for the DMA transfer to complete in flushFrameBuffer()
2022-01-04 7:03 AM
Let me know how it works out for you :)
2022-01-05 2:05 AM
Hi Martin,
I'm pleased to confirm it works pretty well.
What i do is
1) have a flag that is set in sendFrameBuffer() (to indicate a dma transfer is ongoing)
2) wait till this flag is cleared on entry of sendFrameBuffer() (to make sure a second dma transfer won't be started before the current one finish)
3) using the HAL_SPI_TxCpltCallback() to subsequently transfer the next lines required by touchgfx (some static variable are used to keep trace of the current line and other relevant data)
4) clear the flag in HAL_SPI_TxCpltCallback() when there are no more lines to send
i'm printing out the lost frames counter and i definitely see an improvement on it. Which means the cpu is free to proceed further with some touchgfx rendering while a frame is transfered to the lcd.
One remark though:
At first i had a hard time to get the spi working with DMA.
Even something as simple as replacing a blocking call to HAL_SPI_Transmit() with a call to HAL_SPI_Transmit_DMA() followed by a blocking loop to wait the end of the transfer failed:
/* Send the pixels */
//HAL_SPI_Transmit(&hspi2, (uint8_t*)p_buf, size, 100);
HAL_SPI_Transmit_DMA(&hspi2, (uint8_t*)p_buf, size);
while(hspi2.State != HAL_SPI_STATE_READY) {};The spi remained in TX_BUSY state.
with the help of this post: https://community.st.com/s/question/0D50X0000AxEm8U/solved-spi-dma-doesnt-transmit-anything-is-my-configuration-wrong i called MX_DMA_Init() before MX_SPI2_Init(); and this fixed the issue.
It's a bit annoying to redo this change everytime i regenerate the code from STM32cubeMX so it would be nice if you could confirm 1) this is a bug in cubeMX 2) it will be soon fixed
Thanks,
Laurent
2022-01-05 2:57 AM
Aha, that's unfortunate!
I don't have time to confirm, but you could add a call to MX_DMA_Init() inside a user code section that's before MX_SPI2_Init() ?
/Martin
2022-01-05 3:01 AM
well, that's exactly what i did for the time being and it works indeed, but you'll agree it's not the cleanest workaround :)
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* LVE: see https://community.st.com/s/question/0D50X0000AxEm8U/solved-spi-dma-doesnt-transmit-anything-is-my-configuration-wrong
* MX_DMA_Init(); must be called before MX_SPI2_Init(); so we place a call here to avoid to change everytime code is generated from STM32CubeMX
*/
MX_DMA_Init();
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_CRC_Init();
MX_TIM16_Init();
MX_TIM2_Init();
MX_I2C3_Init();
MX_SPI2_Init();
MX_DMA_Init();
MX_TouchGFX_Init();
/* USER CODE BEGIN 2 */Regards,
Laurent
2022-01-05 3:03 AM
I completely agree :) I or @Romain DIELEMAN will report this.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.