2020-06-25 12:13 PM
Even after that I am getting "?????? " from memory address 0x90000000 in memomy browser from STM32Cube IDE. What does that tells?
Can you please guide me in a right direction?
2020-06-26 2:12 AM
How did you create this project?
/Martin
2020-06-29 12:19 PM
Hi Martin,
I created a project in STM32CubeMX :
Toolchain/ IDE: STM32CubeIDE
Board used: STM32F469I-Discovery Board with default settings.
I was trying to step through the How To guide for bringing up a board in the TouchGFX documentation. During "Step 6. External Addressable Flash" I ran into an issue with Hard fault and I was getting "????????" at address 0x90000000 up until the point it was configured.
Thanks to @Community member He Suggested I go through the BSP code for the STM32F469I-DISCO to set up the QSPI suitably. This resolved my issue with the hard fault.
I then loaded the external linker and got the QSPI in build analyzer.
Thank you!
2020-06-29 12:47 PM
Sorry for the late reply.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.