2022-01-12 10:22 PM
Hello everyone,
I have pretty uncommon question. I'm working on STM32WB with SBSFU, and I'm wondering, if it's possible to use non-secure boot with it? As far as I'm concerned, secure boot is enabled by default, but many security features can be disable using flags.
Also, another question: All the provided examples are using USART YMODEM to transfer data. I know, that it really doesn't matter what kind of protocol you use as long as image is placed in a correct place in the memory, but I wonder if I can use DFU feature to update firmware and still use SBSFU. I think it should be possible.
Thank you in advance.
Solved! Go to Solution.
2022-01-13 12:19 AM
Hi,
regarding your first point: SBSFU as a secure bootloader implements two things
(A) check and set-up the STM32 security infrastructure => this you can disable thanks to compiler switches in app_sfu.h.
You can enable SECBOOT_DISABLE_SECURITY_IPS to disable all IPs at once.
This means you won't have code isolation any more for instance.
(B) check the authenticity and integrity of the application before booting it.
This means using crypto services to check the firmware image you have programmed.
This cannot be disabled by compiler switches.
If you want to boot the firmware "blindly" (no check) then you can have a loot at sfu_boot.c to see how the bootloader does that. If you want to disable it then you have to bypass the checks.
Regarding your second point : at boot-up, SBSFU checks the content of the download slot to see if a new firmware image must be installed. You can use any method of your choice to populate this slot. As long as you write the ".sfb" correctly in this slot, it will be detected by SBSFU at boot stage and it will be installed.
Hope this helps.
2022-01-13 12:19 AM
Hi,
regarding your first point: SBSFU as a secure bootloader implements two things
(A) check and set-up the STM32 security infrastructure => this you can disable thanks to compiler switches in app_sfu.h.
You can enable SECBOOT_DISABLE_SECURITY_IPS to disable all IPs at once.
This means you won't have code isolation any more for instance.
(B) check the authenticity and integrity of the application before booting it.
This means using crypto services to check the firmware image you have programmed.
This cannot be disabled by compiler switches.
If you want to boot the firmware "blindly" (no check) then you can have a loot at sfu_boot.c to see how the bootloader does that. If you want to disable it then you have to bypass the checks.
Regarding your second point : at boot-up, SBSFU checks the content of the download slot to see if a new firmware image must be installed. You can use any method of your choice to populate this slot. As long as you write the ".sfb" correctly in this slot, it will be detected by SBSFU at boot stage and it will be installed.
Hope this helps.
2022-01-13 7:20 AM
Yes! This is exactly the answer I was looking for. Thank you :).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.