2025-07-14 11:16 AM
From the manual UM3254:
4.1.4 PSA firmware update service
4.1.4.1 Description
This service provides an implementation of the PSA firmware update API defined in [PSAfwuAPI]. It provides a
standard and platform-agnostic interface for firmware updates.
The firmware update scheme is based on a dual slot: one active slot and one download slot. The active slot is
used to execute the firmware and the download slot is used to download the new image to be installed.
The following images can be updated:
• Nonsecure application
• SMuRoT
• Secure Manager
• Secure modules (each can be updated independently)
The installation flow is as follows:
1. The nonsecure application (update agent) gets information about the installed images (such as name,
installation status, version, and others).
2. It downloads the image to the secure download slot.
3. It requests the image installation. It resets the device to execute the secure boot stages (SMiRoT and
SMuRoT) that perform the installation in the active slot and jumps to the nonsecure application.
4. The nonsecure application must accept the image using its specific acceptance criteria (nonsecure application
dependent):
– If the acceptance criteria are met, the nonsecure application informs the firmware update service that
the image is accepted.
– If the acceptance criteria are not met, the nonsecure application generates a reboot. The secure boot
stages are executed and perform a rollback to the previous valid image, which was swapped in the
download slot.
Two questions:
In step 4, the nonsecure application that must accept the image is already the new application that got installed into the active slot in step 3, correct?
In the last sentence, it sounds as if the SM, while doing step 3 (programming the active slot from the download slot), also copies (backs up) the old application from the active slot into the download slot ("which was swapped") so that when the new application is not accepted, the firmware update service can restore the old application from the download slot. Is this understanding correct? If not, what does the "which was swapped" mean exactly?
Thanks,
Chris
Solved! Go to Solution.
2025-07-15 8:34 AM
Hello @Christian Keydel ,
We have an example in our package X-CUBE-SEC-M-H5, available at https://www.st.com/en/embedded-software/stm32trustee-sm.html
This wiki demonstrates how to use the PSA firmware update service with YMODEM: https://wiki.st.com/stm32mcu/wiki/Security:How_to_start_with_Secure_Manager_customized_config_on_STM32H5#Using_the_PSA_API.
Regarding step 4, the acceptance criteria depend on your own constraints or requirements. For example, you can perform checks on the new non-secure application to ensure all features are still available, verify the version, etc.
Best regards,
Johny
2025-07-15 12:38 AM
Hello @Christian Keydel
Yes, after the reset in step 3, the nonsecure application that boots in step 4 is the new application (let's call it ns_appli_b). The old application (ns_appli_a) is in the download slot and can be swapped if necessary.
You’ve got it right. If ns_appli_b doesn’t meet the acceptance criteria, you can cancel the process and recover ns_appli_a.
Best regards
Johny
2025-07-15 1:53 AM
Hello @JohnyKessler,
Thanks, that is clever.
Is there any example from ST to demonstrate this? Ideally, all steps (e.g. using a USB update agent) but at least how an application does the verification in step 4?
In CubeMX I found the "TFM" series of examples for the STM32L562E-DK that also uses PSA but it is pretty old and I don't know if it still applies. Is there anything newer?
Thanks,
Chris
2025-07-15 8:34 AM
Hello @Christian Keydel ,
We have an example in our package X-CUBE-SEC-M-H5, available at https://www.st.com/en/embedded-software/stm32trustee-sm.html
This wiki demonstrates how to use the PSA firmware update service with YMODEM: https://wiki.st.com/stm32mcu/wiki/Security:How_to_start_with_Secure_Manager_customized_config_on_STM32H5#Using_the_PSA_API.
Regarding step 4, the acceptance criteria depend on your own constraints or requirements. For example, you can perform checks on the new non-secure application to ensure all features are still available, verify the version, etc.
Best regards,
Johny
2025-07-22 2:41 AM
Hello @JohnyKessler,
Thanks again. I am working though this and one important question came up:
What happens if there is a reset or power failure during step 3 (the programming of the active slot with ns_appli_b while swapping ns_appli_a to the download slot)?
Will secure manager keep track of the stage it was in and resume the operation until finished or is the device now hanging in secure manager and needs manual intervention?
Cheers,
Chris
2025-07-23 8:04 AM
Hello @Christian Keydel ,
The SMuRoT automatically resumes from where it left off, whether there is a reset or a power failure during the process. There is no need for manual intervention.
Best regards,
Johny
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.