2022-04-29 2:16 AM
Hi,
In TFM and SBSFU applications, by default the anti-tamper protection is enabled for both internal tamper events and external tamper events. It is activated at the start of TFM_SBSFU_Boot, and remains active.
In case of tamper detection, sensitive data in SRAM2, caches and cryptographic peripherals are immediately erased, and the tamper interruption triggers a reset and the application is blocked (can't boot).
I'm using the anti-tamper protection in TFM with stm32U585, but I don't want the tamper interruption to trigger a reset, I have changed the default configuration in TAMP_IRQHandler(), but still a reset is triggered and the application is blocked at tamper detection, I have tried to catch reset causes (reset flags), and I have found a software reset flag (Set by hardware when a software reset occurs.) and NRST Pin reset flag (Set by hardware when a reset from the NRST pin occurs.), So I wonder what would be the cause of NRST reset, and is there any relation between NRST , TAMP and RTC, could the anti-tamper protection / RTC triggers NRST reset.
Any explanation or a hint, please !
Thank you.
Regards,
ZK.
2022-05-04 1:43 AM
No, Option Bytes should not be affected by the tamper.
Besides, we recommend using RDP-level 2 so the option bytes are frozen in this case.
In RDP-level2 (or production mode), SBSFU only checks the consistency of the OBs.
2022-05-04 2:33 AM
In Dev mode Option Bytes were affected by tamper detection, in Prod mode they should not be affected, So to draw a conclusion :
So the default configuration at tamper detection (forcing a RESET and Reboot) can't be changed !
Thank you.:)
Regards,
ZK
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.