2020-11-23 5:22 AM
I'm trying to finish a first homework related to the SBSFU. I can build the SECoreBin project which at the end generates the SECoreBin.bin file. So it works fine. Next I try to build the SBSFU project but then I get
"Nothing to build for project STM32L476RG_NUCLEO_2_Images_SBSFU"
Building the UserApp ends with an error:
c:\st\stm32cubeide_1.4.2\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.4.0.202007081208\tools\arm-none-eabi\bin\ld.exe: cannot find -l:se_interface_app.o
collect2.exe: error: ld returned 1 exit status
make[1]: *** [makefile:58: UserApp.elf] Error 1
make: *** [makefile:51: all] Error 2
"make all" terminated with exit code 2. Build might be incomplete.All the tools are installed correctly, Java is updated.
Michal
2020-11-23 5:33 AM
Hello Michal,
could you please try again this ?
Select
STM32L476RG_NUCLEO_2_Images_SECoreBin
Clean Project
Build project
Insure to get this trace :
"arm-none-eabi-objcopy -O binary SECoreBin.elf "SECoreBin.bin"
Finished building: SECoreBin.bin
14:27:43 Build Finished. 0 errors, 0 warnings. (took 25s.201ms)"
Select STM32L476RG_NUCLEO_2_Images_SBSFU
Clean Project
Build project
Insure to get this trace :
"
....
arm-none-eabi-objcopy -j .SE_IF_Code "SBSFU.elf" se_inter.elf > /dev/null 2>>1
arm-none-eabi-objcopy --extract-symbol se_inter.elf se_interface_app.elf
arm-none-eabi-objcopy -S --keep-symbols=../se_interface.txt se_interface_app.elf se_interface_app.o
14:30:03 Build Finished. 0 errors, 0 warnings. (took 1m:3s.786ms)"
If it still not working I would advise to delete the 3 project from CubeIDE and erase the the SBSFU folder and restart installation of SBSFU.
I will send you an invitation for a help session ( at 4.00pm) .
Best regards,
Frantz
2020-11-23 6:11 AM
Franz,
Thanks for the quick answer!
So, I tried cleaning projects before building them - it didn't help.
However, I deleted a whole workspace in the Cube IDE and deleted the STM32CubeExpansion_SBSFU_V2.4.0 folder from the STM32SecuWS\L4. Then I created a new workspace and copied again a fresh package to the STM32SecuWS\L4. After that I'm finally able to build everything without any errors.
Thanks a lot for your support!
Michal
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.