2021-10-29 8:30 PM
Hello all,
I have developed a code for stm32f103, which works fine.
During code execution, some device configuration data is Read & written into flash (works fine).
But when i enable read out protection, the code doesn't work.
My understanding is that when read out protection is enabled, code is not able to read/write data from flash, in result it doesn't initialize the configuration parameter of device.
i tried to enable to the read out protection by both ways.
......from st-link utility tool
or
......by writing in code itself.
/***************code for read out protection****************/
uint8_t ReadProtectionConfig(uint8_t ProtectionLevel)
{
uint8_t status = 0;
FLASH_OBProgramInitTypeDef OB_Init;
HAL_FLASH_Unlock();
HAL_FLASH_OB_Unlock();
OB_Init.OptionType = OPTIONBYTE_RDP;
if (ProtectionLevel == 0)
{
OB_Init.RDPLevel = OB_RDP_LEVEL_0;
}
else if (ProtectionLevel == 1)
{
OB_Init.RDPLevel = OB_RDP_LEVEL_1;
}
else
{
status = 1;
return status;
}
HAL_FLASHEx_OBProgram(&OB_Init);
HAL_FLASH_OB_Launch();
HAL_FLASH_OB_Lock();
HAL_FLASH_Lock();
return status;
}
in both case read out protection works ok.
Post edited to adhere community guidelines.
please guide me on this.
2021-10-30 6:04 AM
Have a look at Read protection in PM0075. Read protection also write protects some first pages. Or use a page granular write protection.
2021-10-31 10:07 PM
i am using stm32f103cbt7 in my project which has 128KB of flash ( 0x08000000 - 0x0801FFFF) total 128 pages each of 1KB.
my hex file is using memory from (0x08000000 - 0x080052CB)
i am using last page of flash to write some data (0x0801FC00 - 0x0801FC8B)
And using code for implementing read protection (as mentioned in question / first comment).
what can i do now.
@Uwe Bonnes
2021-11-16 1:49 AM
I am very very sorry for the delay for this post.
i was making a very basic error, but now i have solved this.
"When readout protection is enabled, a POR(power on reset) is required after protection enabled."
Before entering in infinite loop, i was calling the ReadProtectionConfig function for enabling protection.
like this
ReadProtectionConfig(1);
while(1)
{
// further application code
}
so it was requiring a POR every time.
so i changed calling of ReadProtectionConfig function to below code.
if(READ_BIT(FLASH->OBR, FLASH_OBR_RDPRT) == 0) // Checking if protection is disabled
{
ReadProtectionConfig(1);
}
else
{
// Do nothing
}
while(1)
{
// further application code
}
now it is working fine because now ReadProtectionConfig function will be called only one time.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.