2023-02-21 7:24 AM
2023-02-22 5:16 AM
Figured out the problem - the STM32C0116-DK when connected to USB must not be opened by any host app or MCU will detect onboard programmer and hard faults. My shame ;)
2023-02-21 7:30 AM
Hi,
[ ... deleted... ]
Issue is that STLink must not be opened by any host app, see below
2023-02-22 1:31 AM
I'm having two STM32C0116-DK boards. So I've made the simple experiment, unpacked the second board that is shipped with _stock_ LED blinking project and locked it to RDP 1 with :
STM32_Programmer_CLI -c port=SWD freq=4000 -ob RDP=0xBB
Repowered it and guess what ? It stopped blinking exactly as my simple project above. I guess there is real problem with STM32C0 series concerning this issue.
2023-02-22 2:00 AM
Made the same experiment with STM32C0316-DK and all is working as expected - RDP 1 do not crash the firmware. Seems like problem is related at least to STM32C0116
2023-02-22 5:08 AM
Hello @BRusl.1 ,
I did the test with the C011DK, C031DK and NUCLEO, I never observed the issue. I changes the RDP with cube programmer and then after a POR the LED MCU is working fine (LED blinking with HAL delay of 100ms).
Which product revision are you using ? And did you do the POR after changing the RDP ?
BR,
Simon
2023-02-22 5:16 AM
Figured out the problem - the STM32C0116-DK when connected to USB must not be opened by any host app or MCU will detect onboard programmer and hard faults. My shame ;)
2023-02-22 5:23 AM
Mistakes are there to be learned from. ;)
Thank you for finding this and reporting it back here!
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.