2020-08-07 5:52 PM
I have been able to build the STM32H7B3I_DISCO_2_Images_Loader from STM32CubeExpansion_SBSFU_V2.3.0 project targeting STM32H7B3I_DISCO board. I have also been able to build the example file and use the Ymodem protocol for sending the UserApp.sfb file to the the board.
Instead of the Ymodem protocol I am trying to use an I2C master device for sending the UserApp.sfb file. Looking at the example there is a lots of dependencies on the Ymodem protocol.
Is there a way I can determine the file size from the sfb so I can use that in the I2C master for determining the number of bytes that needs to be sent to the STM32H7B3 board.
I am looking for a break down of the sfb data structure, with the hope that I can get information such as the file size etc.
Solved! Go to Solution.
2020-09-23 3:29 AM
Hello,
yes, you have the firmware size information located in the header at beginning of the .sfb file.
The structure of the header is described in se_def_metadata.h in SECoreBin project.
Here is what you need:
#elif (SECBOOT_CRYPTO_SCHEME == SECBOOT_ECCDSA_WITH_AES128_CBC_SHA256)
typedef struct
{
uint32_t SFUMagic; /*!< SFU Magic 'SFUM'*/
uint16_t ProtocolVersion; /*!< SFU Protocol version*/
uint16_t FwVersion; /*!< Firmware version*/
uint32_t FwSize; /*!< Firmware size (bytes)*/
Anyway, you need to adapt the loader.c file and replace Ymodem parts by your own.
Best regards
Jocelyn
2020-09-23 3:29 AM
Hello,
yes, you have the firmware size information located in the header at beginning of the .sfb file.
The structure of the header is described in se_def_metadata.h in SECoreBin project.
Here is what you need:
#elif (SECBOOT_CRYPTO_SCHEME == SECBOOT_ECCDSA_WITH_AES128_CBC_SHA256)
typedef struct
{
uint32_t SFUMagic; /*!< SFU Magic 'SFUM'*/
uint16_t ProtocolVersion; /*!< SFU Protocol version*/
uint16_t FwVersion; /*!< Firmware version*/
uint32_t FwSize; /*!< Firmware size (bytes)*/
Anyway, you need to adapt the loader.c file and replace Ymodem parts by your own.
Best regards
Jocelyn
2020-09-23 4:46 AM
Hi Jocelyn,
Thanks for your response. I have already ported the YModem to I2C and working fine. Many thanks for reply
Regards
onio
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.