2024-09-18 11:44 PM
I am integrating SBSFU with the STM32L496ZG microcontroller and have created a new project. I attempted to generate the SFB file using a customized post-build script from the L476 Simple App example. Although I modified the script paths for my project, the SFB file is not being generated.
The command prompt shows:
Encrypt debug\SBSFU. bin into .\\Binary\\\SBSFU. SFU using AES key from Secure Engine binary
An error message is generated:
Exception: AES CBC encryption requires the Firmware Image size to be a multiple of the AES block size (16 bytes)
Could you please provide guidance on how to resolve this issue?
2024-10-16 11:42 PM
Hi @Jocelyn RICARD ,
as a beginner in SBSFU, I am confused, I was editing the post-build script for L476RG in the script section By this way can I generate an SBSF file .
Regards
Jijo Mathew
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.