2025-05-22 4:41 AM - edited 2025-05-22 6:01 AM
If this thread was not read only i would bring it to life again. @Jocelyn RICARD @EEdwa.1 @Bubbles @Arno1 @Denish_Ribadiya @cyril
After succesfull compiling (NUCLEO-G474RE) SBSFU and uploading UserApp troguh (TERATERM)
\en.x-cube-sbsfu-v2-7-0\STM32CubeExpansion_SBSFU_V2.7.0\Projects\NUCLEO-G474RE\Applications\2_Images
I decided time to do the same in linux, the issue is teraterm doesnt work for linux.
Trying to use minicom:
Adding the simbol for minicom special compilation and recompiling SBSFU
installing minicom
sudo apt install minicom
Reading package lists... Done
Building dependency tree... Done
Reading state information... Done
The following additional packages will be installed:
lrzszminicom uses by default YMODEM lrzsz implementation
The FW update is VERY SLOW (for only 24K) and ends up with incomplete
half update:
full update, it says incomplete:
and the SBSFU console says FW too big
======================================================================
= (C) COPYRIGHT 2017 STMicroelectronics =
= =
= Secure Boot and Secure Firmware Update =
======================================================================
= [SBOOT] SECURE ENGINE INITIALIZATION SUCCESSFUL
= [SBOOT] STATE: CHECK STATUS ON RESET
INFO: A Reboot has been triggered by a Hardware reset!
= [SBOOT] STATE: CHECK NEW FIRMWARE TO DOWNLOAD
= [SBOOT] STATE: CHECK USER FW STATUS
No valid FW found in the active slots nor new FW to be installed
Waiting for the local download to start...
= [SBOOT] STATE: DOWNLOAD NEW USER FIRMWARE
File> Transfer> YMODEM> Send CCCCC
Fw too big
= [SBOOT] STATE: HANDLE CRITICAL FAILURE
= [SBOOT] STATE: REBOOT STATE MACHINE
========= End of Execution ==========
Solved! Go to Solution.
2025-05-30 12:09 AM - edited 2025-05-30 12:12 AM
AI answering questions and posting casino app SPAM , what a time to be alive .
the saddest part is that half of your comment makes sense
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.