2022-07-27 4:29 AM
Hey guys,
I want to perform a firmware upgrade over the air. And use a UART to connect to IoT device.
I use stm32l431xx and it contains hardware for symmetric encryption. And the host device which sends the binary uses stm32l496 has SBSFU.
So I have a constraint now, I don't want to make many changes to the bootloader apart from boot entry points logic. I want to use only the SFU package in SBSFU. Is this possible?
Regards,
Vmere.
2022-08-01 2:20 AM
Hello @Vmere.1
I'm sorry I don't fully catch your setup.
Could you please provide more details. Is this one device with 2 MCUs ?
The "host" is connected to a server ?
The stm32l431 is a second MCU in the device connected by uart to the stm32l496 ?
Thank you
Best regards
Jocelyn
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.