2024-01-07 8:18 PM
Hi
It stated in PM0059 page 16: The value of an option is automatically modified by first erasing the user configuration sector and then programming all the option bytes with the values contained in the FLASH_OPTCR register.
I want to know : What's the user configuration sector? Can you help to point to the right ones in the following table?
Solved! Go to Solution.
2024-01-07 8:27 PM - edited 2024-01-07 8:32 PM
The option bytes and the user configuration sector are one and the same.
I guess technically the option bytes are within the user configuration sector. But that's the only thing in there. They refer to the same location in flash.
2024-01-07 8:27 PM - edited 2024-01-07 8:32 PM
The option bytes and the user configuration sector are one and the same.
I guess technically the option bytes are within the user configuration sector. But that's the only thing in there. They refer to the same location in flash.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.