2022-01-06 12:08 PM
Hi,
Device - STM32H7B3I-DK
SBSFU base Project - STM32H7B3I-DK\Applications\2_Images_ExtFlash
I are using a different flash chip than STM32H7B3I-DK has MX25LM51245G and I am using MX25L51245G
1) I have implemented the flash driver and test with standalone project its working as expected.
2) Tested the code with Images_SBSFU project before beginning of secure code
#if 1
// Test the OCTO flash driver
uint32_t buf_len = 0x100;
uint32_t start_address = EXTERNAL_FLASH_ADDRESS + 0x20000;
uint8_t spibuffer[buf_len];
uint8_t spibuffer_read[buf_len];
volatile uint8_t *flash_area_mm = (uint8_t *) (start_address);
for(int i =0; i < buf_len; i++) {
spibuffer[i] = i;
spibuffer_read[i] = 0xAA;
}
SFU_LL_FLASH_EXT_Init();
SFU_FLASH_StatusTypeDef *pFlashStatus = NULL;
if( SFU_LL_FLASH_EXT_Erase_Size(pFlashStatus, (uint8_t*)start_address, buf_len) == SFU_SUCCESS) {
if (SFU_LL_FLASH_EXT_Write( pFlashStatus, (uint8_t*)start_address, (uint8_t*)spibuffer, buf_len) == SFU_SUCCESS) {
if (SFU_LL_FLASH_EXT_Read((uint8_t*)spibuffer_read, (uint8_t*)start_address, buf_len) == SFU_SUCCESS) {
printf("\r\n FLASH OPERATION COMPLETE \r\n");
}
}
}
if (memcmp(spibuffer, spibuffer_read, buf_len)) {
printf("\r\n FLASH TEST FAILED \r\n");
} else {
printf("\r\n FLASH TEST PASSED \r\n");
}
#endif
/* Launch the Bootloader----------------------------------------------------*/
/*
* This is the beginning of the secure part:
* security mechanisms will be enabled.
* The function below should not return (unless a critical failure is encountered).
*/
(void)SFU_BOOT_RunSecureBootService(); /* no need to take care of the returned value as we reboot in all cases */
/* Security or SecureBoot initialization failure. Force a System Reset */
SFU_BOOT_ForceReboot();Problem :
In SFU_LL_FLASH_EXT_Write which Enables ISR __NVIC_EnableIRQ( OCTOSPI1_IRQn ) immediately causes HardFault_Handler
Thread #1 [main] 1 [core: 0] (Suspended : Breakpoint)
OCTOSPIWriteFlash() at OSPIDriver.c:698 0x800a392
BSP_OSPI_NOR_Write() at stm32h7b3i_discovery_ospi.c:325 0x800a67c
SFU_LL_FLASH_EXT_Write() at sfu_low_level_flash_ext.c:111 0x8009484
SFU_LL_FLASH_Write() at sfu_low_level_flash.c:84 0x80093a2
WriteTrailerHeader() at sfu_fwimg_no_swap.c:75 0x8008ce2
InstallNewVersion() at sfu_fwimg_no_swap.c:647 0x8008d9a
SFU_IMG_TriggerImageInstallation() at sfu_fwimg_no_swap.c:880 0x8008fe6
SFU_BOOT_SM_InstallNewUserFw() at sfu_boot.c:900 0x8007c60
SFU_BOOT_SM_Run() at sfu_boot.c:431 0x80079c8
SFU_BOOT_RunSecureBootService() at sfu_boot.c:202 0x8007a1c
<...more frames...> Any pointer here would be helpful.
Thanks in advance!
2022-01-07 9:40 AM
@Jocelyn RICARD have you seen an issue something like this before?
2022-01-07 11:05 AM
Hello @Community member
I understand you have replaced the MX25LM51245G driver in stm32h7b3i_discovery_ospi $by your own driver.
This is working fine in standalone and at beginning of SBSFU but crash when used inside SBSFU.
This is strange indeed.
You say "In SFU_LL_FLASH_EXT_Write which Enables ISR __NVIC_EnableIRQ( OCTOSPI1_IRQn ) immediately causes HardFault_Handler". Are you sure about this ? Is this something you have added ?
Is MPU activated in your setup ?
Did you try adding a breakpoint in the IRQ Handler ?
Best regards
Jocelyn
2022-01-07 11:08 AM
All the security settings are disabled soon as I call _NVIC_EnableIRQ( OCTOSPI1_IRQn ) it's in hardfault handler. I stepped in assembly as well
2022-01-07 11:24 AM
Hi @Community member ,
OK Thank you.
Well I would first try to get the hardfault details in the Cortex fault status registers to try to locate the issue.
I would check the interrupt stack pointer before activating interrupt and check
Best regards
Jocelyn
2022-01-07 11:38 AM
Thanks will continue debug process and update progress.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.