2024-11-12 5:17 AM
Hi everybody,
I am using a platform that is based on STM32. The developers of this platform have provided to me the firmware image as an encrypted .bin file. When I flash it via USB everything is fine.
Then I change their code and recompile everything using STM32CubeIDE. The produced binary is not encrypted. When I try to flash it, the flashing to the microcontroller fails.
Could it be due to the fact that it is not encrypted?
Note: when I flash my code using the .hex and an st-link everything works well.
Thank you in advance.
2024-11-12 5:24 AM
If the "bootloader" of this device expects encrypted binary, and you give it something else, of course it will fail.
As you've seen, it works when flashed directly over ST-LINK.
2024-11-12 5:29 AM
Thanks for your reply Pavel A.
So I guess I should try to encrypt the binary the same way they do.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.