2021-10-19 6:18 AM
Hi,
I want to block flash memory for writng after programming it. It is important that write protect should not be possible to deassert.
I have read about RDP mechanism, but there is information that on level 2 write protection is permament, but only in case of programming flash from JTAG. I need to know how to block flash for programming from booth JTAG and internal program write access.
2021-10-19 6:33 AM
Don't have any of the flash write/unlock code in your app?
Often bits in Option Bytes, but don't recall an otp/fuse type method
2021-10-19 7:27 AM
Please include your chip number. Write protect options are chip specific, and there are thousands of STM32 chips, but typically they exist.
2021-10-19 9:46 AM
Thank you for answer. The chip number is STM32L562
2021-10-19 1:27 PM
If you have a trusted "bootloader", it can disable access to the flash controller for the "application".
This protection will be effective until next reset, then the bootloader will get control and repeat.
2021-10-19 11:47 PM
I found that sentence in RM:
"WRP areas can be modified through option byte changes while RDP level is less than 2."
Does it mean that WriteProtect is permament if I lock WriteProtect in OptionBytes and then I set RDP level 2?
2021-10-20 7:10 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.