2025-01-28 12:57 AM - last edited on 2025-01-28 1:07 AM by Andrew Neil
How can we map HDPL levels to ST boot/ User Boot / User secure app/ user unsecure app in STM32H573 controller ?
In user flash if I want to place my OEM ROT , OEM uROT, Secure App and Unsecure App, How do I map each HDPL level to corresponding boot or user application ?
2025-01-29 1:01 AM - edited 2025-01-29 1:04 AM
Hi @Vishal58,
Please refer to this knowledge base and this Wiki which can help with your questions.
Thank you.
ELABI.1
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-29 1:45 AM - edited 2025-01-29 1:45 AM
Hi ELABI.1,
I have gone through the links referred by you but could not find the answer for my question.
My use case is to use one boot(single stage user defined) and 2 applications(secure and unsecure) in user flash area.
Say I have allocated Bank 1 HDPL user flash area for my boot and another Bank HDPL user flash area for my secure and unsecure applications.
Now How do I specify that boot is at HDPL level 1 and Secure Application is at level 3S and Unsecure application is at HDPL Level 3NS ?
Thanks & Regards,
Vishal K
2025-01-29 3:49 AM
The definition of HDPL areas is done throw Trusted package creator tool which is part of cube programmer and the image generation process will depend on the mapping in of root project which will be used to configure hide protection levels and debuggability in flash_layout.h after compiling the project the Trusted package creator image generation tool will let you define code size areas for both secure and non-secure applications see this wiki which give more details about the usage of the images templates and scripts without the need to manually set HDLP areas How to start with OEMiRoT on STM32H573 and 563–Arm® TrustZone® enabled - stm32mcu and also this Application note AN6007 can help you.
Thank you.
ELABI.1
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-02-02 11:22 PM - edited 2025-02-02 11:29 PM
Hi,
Thank you for your response.
I understand that mapping is being done using the cube programmer.
Can the user create the mapping on his own without using the cube programmer ?
And can the user have flexibility to avoid using the RSS lib and use his own boot and application with trust zone enabled and OBK area to store secure data ?
Thanks & Regards,
Vishal K
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.