2021-04-20 4:29 AM
Hi all,
I generated the SBSFU file. now i am getting another issue, I was thinking to program the .bin file using CubePrg (DFU method)
so I loaded the .bin file which created using sbsfu, then I set the start address as 0x080000000 or 0x0 and trying to execute, but it says that "Operation exceeds memory limits".
Anyone please could you help me with this?
File size and other information is given below,
Normally .bin file = 70KB
After creating SBSFU .bin file = 607KB
.sfb file is = 71KB
L476RG custom PCB
Thanks
2021-04-28 11:08 AM
Hello Roshan,
The address should be 0x08000000, I think you have one more 0. Is this a typo ?
Yes on this chip, the SBSFU bin file is quite big because if contains the empty download slot before the active slot.
Best regards
Jocelyn
2021-05-03 4:38 AM
Hi @Jocelyn RICARD Thank you for the response,
yes, it is typing mistake. it should be 08000000, There is a problem I am facing, I created a LED blink for another custom board based on L476JGYx it worked really good, once I applied the sbsfu parameters as the which mention in the MOOC part 6 video 4, it wont work, I created the .sfb file as well but the outputs are not working
I followed the following procedures;
Please can you help me to sort out this problem? Custom board connection is made using SPI where D+ and D2 to A11 and PA12. ( as I am new to SBSFU) I hope you have a clear idea about my problem if something is not clear. Please let me know
the problem is it working nicely without SBSFu and once the file created with SBSFU it won't work (Even I can't get the Ymodem protocol update feature as well from the press and hold the boot button).
Regards
Roshan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.