2024-08-02 10:45 AM - edited 2024-08-06 9:34 AM
Hi,
When trying to run a simple TrustZone+UART project generated by STM32CubeMX, the chip raises a HardFault when switching to NonSecure mode. In the HardFault handler, the Cortex-M33 CFSR registrer is set to 0x400, indicating an instruction bus error, and lr set to 0xffff_ffa9 (i.e. raised from non-secure code).
The NonSecure code area's access flags (using the TT instruction etc.) is 0x02be0100 (i.e. should allow NS access) and the MPU is disabled, so that doesn't seem to be the issue. This thread details a similar problem, where the GTZC is protecting some regions of RAM from NS access. However, I've set all entries of MPCBB_SecConfig_array to zero (in the autogenerated MX_GTZC_S_Init() function), and that doesn't solve the issue.
Does anyone know what could cause this, and how to fix it?
Thanks.
Solved! Go to Solution.
2024-08-07 8:43 AM
After more digging:
2024-08-07 6:16 AM
After some more mucking around, I'm also getting the issue on a fresh STM32U5A5 Nucleo-144 devboard. I've made care to disable Secure Area 2 in STM32CubeProgrammer (SECWM2_PSTRT=0xff, SECWM2_PEND=0) yet that also doesn't resolve the issue. SAU_SFSR is zero, and SCB_ICSR indicates only a HardFault is active (0x803). SCB_SHCSR (0x4) and SCB_HFSR (0x4000_0000) also don't have any relevant bits set.
2024-08-07 8:43 AM
After more digging:
2024-08-08 4:07 AM
Hello @980nm ,
Thank you for the detailed explanation and the time investigated in this issue, could you please share your version of MX and the .IOC file used to generate this as well as the version of tools used to try and reproduce the issue from my side as the projects provided in the CubeU5Firmware package doesn't show such behavior.
Regards
2024-08-09 4:17 PM
Sorry for the delay. I'm running STM32CubeMX version 6.12.0, with device package version 1.5.1 for L5, and 1.6.0 for U5. (I did hand-edit the L5 IOC file, as I have an the Nucleo-144 but with a STM32L562 swapped in with some hand-soldering. So I edited the file to make it use the default Nucleo-144 board stuff, but enable the extra features in the L562.)
If you want to know about some other bugs in STM32CubeMX I've come across for this project (these happen in both GNU Makefile and CMake projects):
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.