2026-04-28 3:03 AM
Hey guys!
I am currently working with Secure Boot using ARM TrustZones, Secure and Non-Secure!
I have ***ed up my code majorly hehe, and I cant just Ctrl + Z everything since I have edited in a lot of files and generated code from CubeMX (UART, HAL, HASH etc), is there a smooth way to go back to an older version of the entire folder, for example an older version of NonSecure and Secure etc.
Thanks in advance!
2026-04-28 3:11 AM
Do you use a version control system (VCS); eg, Git ?
2026-04-28 3:41 AM
No, unfortunatley not, I am only using STM32CubeIDE, which is why I came here to ask!
2026-04-28 3:48 AM - edited 2026-04-28 3:56 AM
In that case, no.
This is exactly why Software Version Control Systems (SVCS) exist - so now would be the time to start using one!
Git is probably the most widely used nowadays, although others are available.
GitHub, as the name suggests, uses Git and also provides a hosting service.
GitLab is another, and there are many, many more.
PS:
You can host Git locally, but that's a load of extra work and loses the benefit of having an off-site backup.
2026-04-28 4:43 AM
@KareemAlkhouri202 There is a widely used saying that initially sounds extremely harsh and banal, but contains a great deal of truth and applies again and again to exactly such cases, like unique family photos, password safes ... or software versions like yours: no backup, no mercy.
Anyway, now it's too late, but @Andrew Neil has already given you the most important tips.
Good luck!
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.