2015-02-23 8:51 AM
I am starting using the crypto library and with a STM32F407 device
I don't have the hw hash peripheral and I must use the software library My version: M4_CryptoFW_RngHW_2_0_6.a My codebool Lib_SHA1_hash (uint8_t* hash, uint32_t hash_len, uint8_t* p, uint32_t len)
{
SHA1ctx_stt SHA1ctx_st;
bool result ;
/* Initialize context */
memset (&SHA1ctx_st, 0, sizeof(SHA1ctx_st)) ;
/* Set the size of the desired hash digest */
/* Set flag field to default value */
SHA1ctx_st.mTagSize = 20;
SHA1ctx_st.mFlags = E_HASH_DEFAULT;
result = SHA1_Init(&SHA1ctx_st);
if (result != HASH_SUCCESS) return false ;
result = SHA1_Append(&SHA1ctx_st, p, len) ;
if (result != HASH_SUCCESS) return false ;
result = SHA1_Finish(&SHA1ctx_st, hash, &hash_len);
if (result != HASH_SUCCESS) return false ;
return true ;
}
The library manual say the SHA1_Finish must return the hash value in hash buffer and the length of data written in hash buffer in hash_len
the hash buffer contain correct data but my hash_len is always a random value
(The library is precompiled and I see only the asm code)
2015-02-23 9:21 AM
Perhaps you should pass in a pointer, instead of using the address of a throw away parameter on the stack?
2015-02-23 9:44 AM
Oooooooooooooopsssssssssssss!
Stupid mistake !! It work! thanks Clivebool Lib_SHA1_hash (uint8_t* hash, uint32_t* hash_len, uint8_t* p, uint32_t len)
{
SHA1ctx_stt SHA1ctx_st;
bool result ;
/* Initialize context */
memset (&SHA1ctx_st, 0, sizeof(SHA1ctx_st)) ;
/* Set the size of the desired hash digest */
/* Set flag field to default value */
SHA1ctx_st.mTagSize = 20;
SHA1ctx_st.mFlags = E_HASH_DEFAULT;
result = SHA1_Init(&SHA1ctx_st);
if (result != HASH_SUCCESS) return false ;
result = SHA1_Append(&SHA1ctx_st, p, len) ;
if (result != HASH_SUCCESS) return false ;
result = SHA1_Finish(&SHA1ctx_st, hash, hash_len);
if (result != HASH_SUCCESS) return false ;
return true ;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.