STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H745 sbsfu merge for cm4 and cm7?

I'm successfully implemented IAP for stm32h745. so I wish upgrade to sbsfu.Sbsfu has security firmware upgrade. When i implement for IAP, Firmware file was merged cm4, cm7 binary file using Srecord.If I merge files, won't the integrity of the firmwar...

Resolved! Managing Keys Securely

Hi Team,I am working on a project involving the STM32H5 microcontroller and I am in need of information on how to manage the keys securely for encryption and decryption. I have been unable to find a document that covers this topic specifically for th...

Provisioning Failed

Hello,I am working on Secure Boot for one of the project having the following list of information,Board : B-U585I-IOT02ADevice name : STM32U575/STM32U585Device type : MCUDevice CPU : Cortex-M33 I am trying to boot the device using generated keys with...

jjshant by Associate
  • 1492 Views
  • 0 replies
  • 0 kudos

Hardfault in RDP Level Change

Hello, I am writing code for changing the RDP Level, but I am facing a hard fault trigger in the code:this is the line after unlocking the FLASH_CR_LOCK, and FLASH_CR_OPTLOCK. After unlocking able to change the RDP level to 1 or 2 but as soon the deb...

PoojaAgri by Associate II
  • 2920 Views
  • 5 replies
  • 3 kudos

Resolved! SBSFU SFB update package size question

Hello,I am developing an application on STM32H7 MCU which uses SBSFU bootloader for secure firmware updates. I am trying to combine the SFB update package with some additional data in a single binary file that is sent for the firmware. To make this w...

sute by Associate III
  • 1530 Views
  • 1 replies
  • 0 kudos

SFI Step-by-step on STM32 boards with STM32HSM-V2AE

Hi,I have a STM32HSM-V2AE and I tried to follow de "SFI Step-by-step on STM32 boards". In the part of "HSM programming" I connect the STM32HSM-V2AE to the computer with the smart card reader HID OMNIKEY 3121 but I have the following error:Error: HSM ...

mikel-m by Associate III
  • 1023 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.