STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103xx Option bytes getting corrupted

Hello, I am using STM32F103c6 cortex-m3. I am using 100 micro controllers in various boards. In some around 10 micro controllers, I have seen a issue of option bytes getting corrupted. Even though I am writing 0xA5 to RDP to remove read protection wh...

STM32 H7 crypto lib unable to run ecdh

I am trying to run ECDH p384 operation on STM32H753.Using the STM32 Cryptolib 4.5.0, I get the CMOX_ECC_ERR_MEMORY_FAIL error during the operationI increased the stack size to the maximumI was able to run this using mbedTLS + hardware blocks like RNG...

coolname by Associate II
  • 523 Views
  • 0 replies
  • 0 kudos

stm32l552zeq Nucleo board cannot disable trustzone

Hi, I managed to enable TrustZone by setting the TZEN-bit to 1 like soSTM32_Programmer_CLI -c port=SWD -ob TZEN=1But I can't seem to manage to turn it off the same way. I've tried doing it from the graphical interface as well, with the same results. ...

krook by Associate II
  • 648 Views
  • 1 replies
  • 0 kudos

Resolved! Flash Data lost on OPTIONBYTE_WMSEC

Hello!Using h563zi I am trying to update the second bank firmware using an application that has a Secure Part (sectors 0-9) and a Non Secure part with Trust Zone enabled. For easier maintenance the update is done from the Non-Secure part.Settings:SEC...

Resolved! Secure Manager PSA Firmware Update Service

From the manual UM3254:4.1.4 PSA firmware update service4.1.4.1 DescriptionThis service provides an implementation of the PSA firmware update API defined in [PSAfwuAPI]. It provides a standard and platform-agnostic interface for firmware updates.The ...

Tamper Detection on STM32H753

Hello,I try to implement a tamper detection for my project. In general, it works. When the device is only powered by a coin cell and a tamper is detected, the backup registers are erased and unfortunately also the backup RAM. When the device is power...

toni2 by Associate
  • 1753 Views
  • 2 replies
  • 0 kudos

Resolved! How to set RDP level 1 via software on STM32G030

I would like to increase the code readout protection level from 0 to 1 programmatically in an STM32G030.  I must be doing something silly and if anyone sees it, I'd be grateful.  I've stepped through it with the debugger and the flash and option byte...

DAlbe.3 by Senior II
  • 10714 Views
  • 15 replies
  • 2 kudos

Resolved! ST wiki missing page for STM32N6 Security

Hello,It seems to me that the wiki page: https://wiki.stmicroelectronics.cn/stm32mcu/wiki/Security:Secure_storage-SAES_key_wrapping_for_STM32N6 is unavailable as I get the message: "Page not found".I tried searching for it, to no avail. Is the relate...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.