STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 and CyaSSL - Hardware Crypto and RNG Support

Posted on December 28, 2012 at 00:34Hi, We would like to announce that the CyaSSL embedded SSL library now has support for hardware-based cryptography and random number generation offered by the STM32F2.  Supported cryptographic algorithms include A...

STM32F2 SHA1 Hashing

Posted on December 13, 2012 at 22:31Hi,I am trying to integrate STM32F2 SHA1 support into an existing crypto API that is structured with three main functions:sha_initsha_updatesha_finalIt appears from the STM32F2 SHA1 example code that the HASH proc...

CRC Module

Posted on October 01, 2012 at 15:44Hello Is there any difference between the CRC module at STM32F1 Series and STM32F3 Series.? I saw that there are some new registers active and some new features possible ! #crc #crc #crc

acelec by Associate II
  • 5108 Views
  • 8 replies
  • 0 kudos

USB Corrupt CRC in packet

Posted on September 05, 2012 at 22:44I have a situation where the registers appear to be set up correctly, but when I put data into a transmit FIFO, the output on the USB wires is a single byte with a checksum of 0x0000. Put many bytes into the FIFO...

allan2 by Associate
  • 1522 Views
  • 1 replies
  • 0 kudos

STM32F107 bootloader with CRC check of bin files

Posted on July 17, 2012 at 16:38Hi, I've implement bootloader IAP with UART. the code run without any problem and I have software upgrade support to my project. I'm using IAR for ARM v6.40.2, I've tried to use the Linker configuration to generate bi...

tamir23 by Associate
  • 1564 Views
  • 1 replies
  • 0 kudos

Wrong RXCRC for SPI3 with 18Mhz

Posted on April 03, 2012 at 11:57I've interesting behavior on STM32F105VC. I have SPI3(remmaped) master with SPI auto CRC calculation (RXCRC,TXCRC). For 9Mhz it is fine, for 18Mhz I receive all words correct, including CRC, but RXCRC register is wr...

0690X00000602kUQAQ.jpg 0690X00000602gjQAA.jpg
stst9184 by Associate II
  • 2803 Views
  • 7 replies
  • 0 kudos

SPI CRC calculation for polynom 0x8005

Posted on March 23, 2012 at 19:09 I'm lost with my calculation of crc for 16 bit transmit mode, with a polynom 0x8005, init = 0x0000. I am calculating in Matlab a lookup table first, which seems all right: 0000 8005 800F 000A...

stst9184 by Associate II
  • 1269 Views
  • 1 replies
  • 0 kudos

STM32F105 Read protection issue

Posted on February 18, 2012 at 21:29Hello guys. I was trying to read the code out of a STM32F105RBT6 using a SWD circuit and the STMprog software but the code was ''Read protected'' and I couldn't bring it out .Can you guys give me a help or suggest...

vdsr81 by Associate II
  • 3449 Views
  • 6 replies
  • 0 kudos

Export Restrictions for STM32F2

Posted on February 17, 2012 at 14:46Hi, I'm interested in using the cool STM32F2 devices.  Some of them also contains symmetric key cryptographic support.  Does this mean that they fall under the Wassenaar Agreement? #crypto

encryption libraries not working

Posted on February 09, 2012 at 21:59Hi everybodyI'm trying to use the encryption libraries with an STM32F4Discovery board.However, the function HASH_SHA1 is not obtaining the hash value, it only got zero.I am using this code to obtain the hash:====...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.