STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Secure and Encrypted Boot support on STM32F7

Hi,We are using STM32F769BIT6 based system for our product. We like to enhance the system with security.Is it possible to add secure boot and encrypted boot to the system without any hardware modification?

Jith cr by Associate II
  • 904 Views
  • 0 replies
  • 1 kudos

Resolved! SBSFU with FreeRTOS causing FIREWALL RESET FAULT

Hi everyone,I am using STM32L4A6 with FreeRTOS running on it. I integrate SBSFU according to UM2262 and AN5056. After jumping to application, the firmware triggered Firewall reset when calling osKernelStart() .I already turned SysTick off before jump...

SL61 by Associate II
  • 3859 Views
  • 8 replies
  • 0 kudos

Resolved! Firmware image size required for AES CBC encryption

I am trying out the sample projectSTM32CubeExpansion_SBSFU_V2.2.0/Projects/NUCLEO-H753ZI/Applications/1_Image.I have completed the following build steps:prebuild.pyBuild SECoreBinBuild SBSFUBuild UserAppThe last step postbuild.py (which is SECBOOT_EC...

chuan_lee by Associate II
  • 2910 Views
  • 4 replies
  • 0 kudos

Hardware AES 256 CBC Incorrect results

Hi,I am new the the development and I have been testing the hardware aes module.I have tested against a known vector and the results differ from what is expected, I have checked the test vectors using AES provider in .NET and I get the results I expe...

POliv by Associate III
  • 3956 Views
  • 5 replies
  • 0 kudos

STM32F412 CRC32 uint8_t array as input.

Hi,I have (for example) a byte array with the size of 6. Now I want to calculate its crc32 value. The first 4 bytes are no problem - I put them in as word, but what about the last 2 bytes?Thanks for the Help in advance.BRNico

NKorn.12 by Associate II
  • 2035 Views
  • 2 replies
  • 0 kudos

Resolved! Secured boot with a secured & non-secured application

Hello,I now understand that I should have asked the question differently.Let's say we have 2 applications: secured and non-secured application.The secured is placed in inetrnal flash, just as done in the demo of SBSFU,But the non secured should be pl...

ranran by Senior II
  • 3254 Views
  • 9 replies
  • 0 kudos

sha1_alt.c (mbedTLS implementation) bug?

I have a file from ST, not sure where it comes from but the header has:sha1_alt.c for SHA1 HASHCopyright (c) 2017, STMicroelectronicsI am getting issues with the function that call HAL_HASH_SHA1_Accumulate function.They are no checking for size/len i...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.