STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Best practice with SBSFU when manufacturing

SBSFU considers the secure boot as the root of trust. If we develop the firmware and manufacture the products in a factory (I assume that the firmware should be programmed during the manufacturing in the factory), how to guarantee the secure boot is ...

Zoey by Associate III
  • 1285 Views
  • 1 replies
  • 0 kudos

Large application image

I have a large application image running on the STM32F427. The image is more than 1M bytes, which make it impossible for dual-image. From ST's document, for single-image, "The user application cannot download a new firmware image: the local download ...

Zoey by Associate III
  • 1559 Views
  • 2 replies
  • 0 kudos

stm32 cryptographic library

i want to get the stm32 cryptographic library and i request it. but after a week no response received. what should i do?please help me.best regards

mzere by Associate
  • 923 Views
  • 1 replies
  • 0 kudos

Resolved! TeraTerm not showing printouts

I have asked this on ST Online Support. I think I should ask it here too.I use System Workbench to 'build all' 2 big packages "as is":STM32Cube_FW_H7_V1.5.0/Projects/STM32H743I-EVAL/ApplicationsSTM32CubeExpansion_SBSFU_V2.2.0/Projects/NUCLEO-H753ZI/A...

chuan_lee by Associate II
  • 2469 Views
  • 2 replies
  • 0 kudos

Sample project 1_Image postbuild.sh arguments

I am trying to build and flash sample project from:STM32CubeExpansion_SBSFU_V2.2.0\Projects\NUCLEO-H753ZI\Applications\1_ImageI have been able to build the modules -- SBSFU, SECoreBin and UserApp -- from Makefiles using GNU ARM toolchain.SECoreBin/GN...

chuan_lee by Associate II
  • 2362 Views
  • 4 replies
  • 0 kudos

Single Image Download on Dual Bank MCU

Hi,I've some problem in understanding why it's not possible to use the single image download on Dual Bank MCU, as "reported" in the following picture (ref. UM2262 pg.54 par. C.2 Mapping Definition).Could someone give me more details about this limit...

0690X000008aFnlQAE.png
SScla by Associate II
  • 1087 Views
  • 1 replies
  • 0 kudos

SBSFU v2.2.0 on B-L475E-IOT01A

I would like to build the SBSFU demo application for the B-L475E-IOT01A on a linux platform, but i can't find any instructions in the documentation or Makefile to do this.

OAber by Associate II
  • 1203 Views
  • 1 replies
  • 0 kudos

Hello!How can i porting the X-CUBE-SBSFU(V2.20) to STM32G070?

FLASH memory protection is different between STM32G070 and STM32G071.But there is no stm32g070 in the sample project of x-cube-sbsfu package, only stm32g071.Based on project NUCLEO-G071RB, I commented out two protections and compiled them. I wonder i...

0690X00000ApPJFQA3.jpg
wyett by Associate
  • 1710 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.