STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Bricked STM32F446 after unprotect

After testing Proprietary code readout protection (PCROP) features, STM32F4 got bricked.Steps to reproduce:Enable SPRMOD for PCROP usage and enable PCROP bit 3 (Flash sector 3)Send an :unprotect:force DFU commandSTM32 will be bricked by now, not boot...

VictorPr by Associate II
  • 1398 Views
  • 1 replies
  • 0 kudos

STM32L431 Software CRC

Hello, does anyone know how to programmatically calculate a CRC using the same algorithm than the one provided by the CRC module of STM32L431 ? Can ST just provide a up-to-date documentation/application note providing the implement CRC algorithm on S...

ABlam.1 by Associate
  • 1038 Views
  • 0 replies
  • 0 kudos

Resolved! SPI DMA CRC transmit

hi,my type is stm32f031, i try to debug ' spi + dma + crc' mode. i have no idea about transmit crc .i just enable crc_en, and set the bit crc_next every sending 8bit value.my logic analyzer occured the only 8 bit datas, it not contains the the crc va...

Jseyn.1 by Associate III
  • 2594 Views
  • 2 replies
  • 0 kudos

Problem running SBSFU with Keil RTX5 (RTOS)

I am trying to adapt an existing project that uses Keil RTX5 (RTOS2) which was written in C++ to include SBSFU functionality. So far I have got the project to build. However I am not sure about the integrity of the build as Micro-lib does not support...

onio by Senior
  • 2107 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.