STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Dear STM32 Community, I am using : STM32H7xx HAL Driver version number V1.9.0 WolfSSL on a STM32H753, Crypto hardware accelerator not working for TLS

I am trying to use AES-GCM with the crypto hardware accelerator the normal Testvectors are working, but when I connect it to openssl the authentication Tag is wrong. Do you have any idea how to fix this? The normal Encryption in ECB is working. If I ...

AMuen.1 by Associate
  • 1579 Views
  • 1 replies
  • 0 kudos

SBSFU debug along with the Application

Hi,I am facing some issues with debugging SBSFU project.When I flash the application in debug mode, I can not jump to breakpoints set in SBSFU projects.Is there any way to perfrom this.Best Regards,Ankush Nagaraju

ANaga.2 by Associate II
  • 1587 Views
  • 1 replies
  • 0 kudos

Resolved! memory map adjust SBSFU on a STM32G474

HiI'm using the dual image function on a 512kB STM32G474. I like to adjust the bootloader size to 32kb because my user App is too big.In the AN5056 there is a note how to adjust it, but I'm not sure if this lines in the file low_level_security.h are ...

dominik by Senior
  • 7047 Views
  • 20 replies
  • 0 kudos

trying to import one project to cubeide 1.5

Project imported: D:\Vrund\STM32CubeExpansion_SBSFU_V2.4.0\Projects\STM32F413H-Discovery\Applications\1_ImageIssue faced:15:42:35 **** Build of configuration Debug for project STM32F413H_DISCOVERY_1_Image_SECoreBin ****make all Building file: D:/Vrun...

vrund by Associate II
  • 2109 Views
  • 3 replies
  • 0 kudos

Resolved! LIN Bus example on any family of STM32 MCU's

Hello. For my automotive project I need to imitate motorcycle handlebar that uses LINbus for buttons many buttons. Since I can't always take handle off motorcycle I need to make emulator of it.This is Typical frame, and I mapped all bits of this burs...

0693W000007EEX0QAO.png
Linas L by Senior II
  • 11459 Views
  • 1 replies
  • 1 kudos

G070 programming issue?

Hi,Have a code that modifies the option bytes on G0 micro which seems bricks the IC from further programming attempts aka device locks itself.Did anyone face a similar issue with G070? What are the solutions to make the programming process robust and...

sg1 by Associate
  • 2251 Views
  • 3 replies
  • 0 kudos

Modification in SBSFU

I have signature of my user app and user app in .bin format.if i have to use only these two inputs, what modification i need to do in SBSFU? and under what files?i dont want to use post built .bat and prebuilt.bat.i am using Single slot image example...

vrund by Associate II
  • 2674 Views
  • 5 replies
  • 0 kudos

Resolved! STM32L562 sbsfu queries

Hello,I want to use sbsfu for STM32L562 controller with STM32Cube IDE version 1.5.AS per primary research i am using below package and project .I am using STM32SecuWS package.Under that project I am using is STM32SecuWS\TFM\STM32Cube_FW_L5_V1.3.0\Pr...

vrund by Associate II
  • 4537 Views
  • 9 replies
  • 0 kudos

Resolved! Port fails on __IS_SFU_RESERVED()

Hi,I've been trying to port the STM32H753 SBSFU project to the STM32H735G-DK.The bootloader fails in SFU_BOOT_Init due to failing SE_Init().This is the result of __IS_SFU_RESERVED() failing it's test: 0x08008A00 < 0x08008061 < 0x0801FFFF (SB_REGION_R...

Arno1 by Senior
  • 1948 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.