STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STSAFE Provisioning

Hi everyone,I’m using the B‑U585I‑IOT02A development board for an IoT project. The onboard STSAFE‑A110 secure element comes pre‑provisioned with a default key and certificate, but for my application I need to:Provision my own keypair and certificate,...

macar by Associate II
  • 366 Views
  • 1 replies
  • 0 kudos

how to create a NS calibration section

Hello together,I search for a solution to put calibration data in a NS area.Background Information:we are using STM35H573 with STM secure manager.we use an ethernet Rest API to update Application including request install and so onNow I want to use t...

Setting H5 security from firmware

Hi,I added some follow-up questions to a message but I'm not sure if anyone will notice as I had already clicked "Accepted Solution" :-https://community.st.com/t5/stm32-mcus-security/stm32h5-simple-security-settings/m-p/885235/thread-id/9530#M9531Cop...

JimJW by Associate III
  • 311 Views
  • 2 replies
  • 2 kudos

Resolved! STM32H5 simple security settings

Hi,I have a question about choosing some fairly basic security settings for an STM32H5.We are developing a system that uses both G4 and H5 micros. We have developed a largely common bootloader that receives a signed encrypted application over various...

JimJW by Associate III
  • 552 Views
  • 4 replies
  • 0 kudos

Resolved! OEMiROT: what is the expected use case?

Typical bootloaders (including some of ST's built-in bootloaders for other processors) typically allow a code image to be loaded into the processor via some kind of serial link (UART, SPI, CAN, etc), without needing an ST-Link or other debug hardware...

Firmware Protection

Hello Team,We have faced the Firmware ( hex file ) theft by Reverse engineering , Our competitor 2 Times. Yes, Two times , while RDP1 is set. We do not have contarct Manufacture in our whole process.Even Reading / Comparing intertlock of 96 bit UID f...

bsuthar by Senior
  • 683 Views
  • 5 replies
  • 1 kudos

Secure Boot and Secure Update Software Options

Hi, I'm building a medical device that will use an STM32 MCU and requires secure boot and secure firmware updates (over USB-C preferably). I have little experience with implementing secure bootloaders, and am looking for a solution that could allow m...

desaisam by Associate II
  • 730 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.