2026-02-26 2:36 PM - last edited on 2026-02-27 2:00 AM by Andrew Neil
In the documentation on STM32N657X0, it says that the memory must be connected with match length track on the boards.
It says:
Match length (including BGA package length)
- DQS0 with IO0..7 (Byte0), all in 50 mils,
- DQS1 with IO8..15 (Byte1), all in 50 mils,
- CLK is100 mils from any signal of Byte0 or Byte1
- NCS can be CLK +/-700 mils
But I can't find any documentation on "BGA package length".
It seems reasonable that the BGA package should be taken into account, since it is 12.8 mm.
and a precision of 1.27mm (50 mils) is specified.
I hope someone can help me find that documentation.
Keld
Solved! Go to Solution.
2026-03-02 6:25 AM - last edited on 2026-03-02 6:36 AM by Andrew Neil
Hello @Keld and welcome to the community;
The VFBGA package dimensions are illustrated in DS14791 Rev 9 precisely section "6 Package information".
Regarding the comments on length equalization in our STM32N6570-DK and NUCLEO-N6570X0Q board schematics, the BGA package lengths mentioned in the comment likely refer to an older design that is not necessarily related to the STM32N6.
Here are the routing recommendations:
1- the die bumps to package balls substrate length is not released to customers as the package skew is considered negligible for xSPI frequencies. Therefore, they do not need to be taken into account.
2- The 50 mils specification can be extended to a matching length of 200 mils for all XSPI signals and that if the external memory is on the same PCB as the STM32N6, then the physical dimensions of the package can be neglected in the sizing.
3- Finally, as a recommendation, you can be in charge of the PCB design refer to the IBIS models containing the die IO + package models for xSPI signal integrity simulations and check to ensure results are within specifications.
The STM32N6 Ibis model files for all packages are available in the link below:
https://www.st.com/en/microcontrollers-microprocessors/stm32n6-series.html#cad-resources
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-03-02 6:25 AM - last edited on 2026-03-02 6:36 AM by Andrew Neil
Hello @Keld and welcome to the community;
The VFBGA package dimensions are illustrated in DS14791 Rev 9 precisely section "6 Package information".
Regarding the comments on length equalization in our STM32N6570-DK and NUCLEO-N6570X0Q board schematics, the BGA package lengths mentioned in the comment likely refer to an older design that is not necessarily related to the STM32N6.
Here are the routing recommendations:
1- the die bumps to package balls substrate length is not released to customers as the package skew is considered negligible for xSPI frequencies. Therefore, they do not need to be taken into account.
2- The 50 mils specification can be extended to a matching length of 200 mils for all XSPI signals and that if the external memory is on the same PCB as the STM32N6, then the physical dimensions of the package can be neglected in the sizing.
3- Finally, as a recommendation, you can be in charge of the PCB design refer to the IBIS models containing the die IO + package models for xSPI signal integrity simulations and check to ensure results are within specifications.
The STM32N6 Ibis model files for all packages are available in the link below:
https://www.st.com/en/microcontrollers-microprocessors/stm32n6-series.html#cad-resources
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-03-02 6:37 AM
@KDJEM.1 wrote:the BGA package lengths mentioned in the comment likely refer to an older design that is not necessarily related to the STM32N6.
So will you be updating the document to reflect that?
2026-03-03 12:41 AM
Hello @Andrew Neil ;
A request to remove these comments from the STM32N6570-DK and NUCLEO-N6570X0Q boards schematics is submitted internally.
Internal ticket number: 228170 (This is an internal tracking number and is not accessible or usable by customers).
Thank you for your contribution in STCommunity.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.