2017-07-18 12:26 AM
I'm trying to write application on the STM3210C-EVAL that will open multiple tcp connections.
I've started with the VisualGDB STM32 CubeMX sample LwIP_TCP_Echo_Client sample
and it works on my eval board (the application connects to my demo tcp server)But I want to use sockets, I don't want to have to manage the packets.
I've tried to compile the LwIP with support for sockets but I can't get it to compile.The flags I've set in lwipopts.h are:
#define LWIP_TIMEVAL_PRIVATE 0
#define LWIP_NETCONN 1#define LWIP_SOCKET 1When I try to compile I get an error that lwip/netbuf.h does not exist.
Is there a way to use sockets with lwip 1.4 or is it not supported?
Thanks,
Nadav2017-07-18 3:16 AM
Hello
nadavp
,The last version of STM32CubeF1 supported LwIP v2.0.0
Have a look to the UM1713 manual for more details about LwIP: “Developing applications on STM32Cube with LwIP TCP/IP stack“.
With Regards
Imen
2017-07-19 4:19 AM
Hi Imen,
Thanks for your reply,
I've been reading the UM1713 document and it looks very promising
Especially the example of TCP echoserver demonstration using the Netconn API looks good.
Is there some place where I can download the sources of the examples in the document?
Thanks,
Nadav
2017-07-19 5:12 AM
Hi
nadavp
You can download the
from STMicroelectronics official site, then you find the '
LwIP_TCP_Echo_Server'
example at this path:STM32Cube_FW_F1_V1.6.0\Projects\STM3210C_EVAL\Applications\LwIP\LwIP_TCP_Echo_Server
Regards
Imen
2017-07-19 5:34 AM
Hi Imen,
In the UM1713 there is a discussiong of an example of a Tcp echo server using netconn API (section 5.2.2)
This example does not seem to be included in the STM32CubeD1 v1.6
(the LwIP examples included with
STM32CubeD1 v1.6 are using LwIP Raw API without RTOS )
Thanks,
Nadav
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.