2025-11-08 5:46 AM - last edited on 2025-11-10 5:51 AM by Imen.D
I just spent some time debugging a fundamental compatibility issue between an MPU and its RAM, and I wanted to share what I learned to save others the same headache.
I was looking at using the STM32N657 (a powerful Cortex-A7 MPU) and almost made a critical error by assuming it could work with a common SDR SDRAM chip like the W9825G6KH-6.
Spoiler Alert: It can't. Here's why.
The STM32N657 has a DDR3/LPDDR2/LPDDR3 memory controller. The W9825G6KH-6 is an SDR SDRAM. These are two completely different, incompatible memory technologies.
Think of it like trying to put diesel fuel in a gasoline engine. Both are fuels, but the underlying technology and "communication protocol" are entirely different.
Post edited by ST moderator to update the wrong product name "STM32MP657" to "STM32N657".
2025-11-08 6:05 AM
Huh?
> STM32MP657
The STM32MP657 doesn't exist. Probably meant STM32N657?
> The STM32MP657 has a DDR3/LPDDR2/LPDDR3 memory controller. The W9825G6KH-6 is an SDR SDRAM. These are two completely different, incompatible memory technologies.
STM32N657 definitely support SDRAM. It can work with the W9825G6KH-6 in SDR mode.
2025-11-08 7:12 AM
Sorry
Yes im looking for STM32N657
2025-11-08 7:17 AM
I need support for developing a custom bord with maximum external ram and flash setup , bootloader and air application setup
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.