2016-03-24 1:46 PM
I am developing a low power application for the stm32L151RC and after a lot of debugging noticed that the system_stm32l1xx.c file does a
RCC->CR |= ((uint32_t)RCC_CR_HSEON);Why would it do that. Why not just continue with the MSI at 2 MHz?Now my application consumes to much power during sleep mode (1.64 mA instead of 150uA).I know I can simply alter the systemInit function, but why does it do this in the first place?2016-03-24 2:11 PM
The system_stm32l1xx.c is expected to be modified to suit the board/application.
Perhaps the availability of a faster more accurate clock was desirable for the applications they had in mind? CAN or USB perhaps?Trying to understand ''why'' ST does certain things will just give you a headache, I'd recommend you figure what it is you want to do, and then do that thing.2016-03-24 2:18 PM
Ah, my mistake.
I was used to MCU's designed for low power actually being used for low power applications. ;)We’re moving the ST Community to a new platform to give you a better and more reliable community experience.