2023-07-20 4:30 PM - edited 2023-07-20 5:01 PM
System: STM is set to use a PLL fed by MSI. The PLLM is set to 6 and the MSI to 48 MHz.
Issue: When HAL_PWREx_EnterSHUTDOWNMode is executed, the processor should stop executing instructions after this command. Yet occasionally it goes past it indicating it did not successfully enter shutdown mode. This caused the processor to get stuck in an while(1).
Description:
Fix:
Was anyone able to have it flawlessly enter shutdown mode on the first try?
void HAL_PWREx_EnterSHUTDOWNMode(void)
{
/* Set Shutdown mode */
MODIFY_REG(PWR->CR1, PWR_CR1_LPMS, PWR_CR1_LPMS_SHUTDOWN);
/* Set SLEEPDEEP bit of Cortex System Control Register */
SET_BIT(SCB->SCR, ((uint32_t)SCB_SCR_SLEEPDEEP_Msk));
/* This option is used to ensure that store operations are completed */
#if defined ( __CC_ARM)
__force_stores();
#endif
// @CABAN EDIT: ensure memory synchronization
__DSB();
/* Request Wait For Interrupt */
__WFI();
}
void hal_deepsleep(void)
{
// @CABAN EDIT: set MSI to f < 16 MHz, per errata document section 2.5.13
// reset clocks: MSI sysclock, MSI at 4Mhz
HAL_RCC_DeInit();
HAL_Delay(1);
// Disable IRQs
core_util_critical_section_enter();
// Stop HAL tick
HAL_SuspendTick();
uint32_t EnterTimeUS = us_ticker_read();
// Request to enter SHUTDOWN mode with regulator in low power mode
#if TARGET_STM32L4
int pwrClockEnabled = __HAL_RCC_PWR_IS_CLK_ENABLED();
int lowPowerModeEnabled = PWR->CR1 & PWR_CR1_LPR;
if (!pwrClockEnabled) {
__HAL_RCC_PWR_CLK_ENABLE();
}
if (lowPowerModeEnabled) {
HAL_PWREx_DisableLowPowerRunMode();
}
// @CABAN EDIT: Use STM Shutdown mode for deep sleep.
// Upon wake up, the system will be subject to a silicon-forced reset.
// instruction after HAL_PWREx_EnterSHUTDOWNMode shall not be executed.
HAL_PWREx_EnterSHUTDOWNMode();
/* CPU should not reach this execution point. Reset if CPU get here */
NVIC_SystemReset();
/* CPU shall not rech this execution point */
if (lowPowerModeEnabled) {
HAL_PWREx_EnableLowPowerRunMode();
}
if (!pwrClockEnabled) {
__HAL_RCC_PWR_CLK_DISABLE();
}
#else /* TARGET_STM32L4 */
HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);
#endif /* TARGET_STM32L4 */
// Restart HAL tick
HAL_ResumeTick();
// Enable IRQs
core_util_critical_section_exit();
// After wake-up from STOP reconfigure the PLL
SetSysClock();
TIM_HandleTypeDef TimMasterHandle;
TimMasterHandle.Instance = TIM_MST;
__HAL_TIM_SET_COUNTER(&TimMasterHandle, EnterTimeUS);
#if DEVICE_RTC
/* Wait for RTC RSF bit synchro if RTC is configured */
#if (TARGET_STM32F2) || (TARGET_STM32F4) || (TARGET_STM32F7)
if (READ_BIT(RCC->BDCR, RCC_BDCR_RTCSEL)) {
#else /* (TARGET_STM32F2) || (TARGET_STM32F4) || (TARGET_STM32F7) */
if (__HAL_RCC_GET_RTC_SOURCE()) {
#endif /* (TARGET_STM32F2) || (TARGET_STM32F4) || (TARGET_STM32F7) */
rtc_synchronize();
}
#endif
}
2023-07-23 7:49 AM - edited 2023-07-23 8:01 AM
All of the related ST's code is broken and they are not even capable of understanding it:
And the same is true for Stop modes:
https://community.st.com/t5/motor-control-mcu/mc-sdk-not-work-with-mcu-stop-mode/m-p/94522
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.