2016-03-24 5:50 AM
ST wrote in ReadMe:
In order to program the demonstration you must do the following:
1- Open STM32 ST-Link Utility V3.7, click on ''External Loader'' from the bar menu then check
''N25Q128A_STM32F746G-DISCO'' box
2- Connect the STM32746G-DISCOVERY board to PC with USB cable through CN14
3- Use ''STM32CubeDemo_STM32746G-DISCO_V1.1.0.hex'' file provided under “Binary�? with STM32 ST-Link Utility
to program both internal Flash and external QSPI memory
4- copy the audio and video files provided under ''Utilities/Media/'' in the USB key
5- Plug a USB micro A-Male to A-Female cable on CN12 connector
-> The internal Flash and the external QSPI are now programmed and the demonstration is shown on the board.
How could 4th point be done? There is only 1 Mb flash and no way to simply copy on disk.
And what about CN12 connect? What is it for?
2016-03-24 3:48 PM
Translation:
You put the files on a USB Flash Drive, that *you* supply, and you plug it into the DISCO board's USB HS port (CN12) with an adapter cable that you also supply.2016-03-24 3:54 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.