2018-07-13 1:04 AM
Why is the STM32WB series UART only two?
2018-07-13 1:46 AM
Probably because that was sufficient to meet a primary customers goals in the available package and pins.
This is an old design there are newer F4 based designs now, and alternate modules.
2018-07-16 12:45 AM
In my usage scenario, you need a UART to communicate with the RFID module, another UART communicates with the 2D-code scanning engine, and a third to do the debug print and IAP
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.