2020-12-22 10:25 AM
I'm using the STM32F072RB MCU and I am trying to increase the SPI baud rate. The HSI48 Clock is 48MHz and the minimum SPI clock prescaler is 2 which comes out to be 24Mbit/s. However, it gives me an error stating that the baud rate is more than 18MBit/s. Why is this and is there anyway to change it?
Solved! Go to Solution.
2020-12-22 1:57 PM
This is the limit given in DS, see SPI/I2S characteristics chapter.
So no, you can't change it, learn to live with it.
JW
2020-12-22 1:57 PM
This is the limit given in DS, see SPI/I2S characteristics chapter.
So no, you can't change it, learn to live with it.
JW
2020-12-22 4:22 PM
Or replace the chip with one that can do 24 MHz. Plenty of them out there.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.