2020-05-31 2:41 AM
Hi, I configured PWM 25 kHz on Nucleo-767ZI to control the PWM fan.
When I set up Duty Cycle 1% -3% and 98% -99% the PWM signal is deformed.
When the Duty Cycle is 4% to 97% PWM signal is good.
Can it be improved or is it normal?
Regards
2020-05-31 4:04 AM
That's your oscilloscope's inability to trigger on short pulses, or maybe it's set so (search for "HF rejection, noise rejection" in Trigger settings).
JW
2020-06-01 5:44 AM
This is normal for pwm. Designers often use 5%-95%.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.