2022-04-12 8:39 PM
I want to make robotic arm , CNC controller for this purpose which STM32 is capable to do DSP, arithmetic and floating point calculation Faster (less clock cycle for execution)without much execution code delay?
So interpolation and trigonometric functions execute faster and machine axis runs without any leg in calculation.
Suggest me any DSP or MCU ic available which can perform above task.
2022-04-12 9:32 PM
Probably the STM32H725/735, has double and single precision FPU, clocks at 550 MHz. The FPU itself does not support transcendental functions directly, for that you'd perhaps look at Intel Atom or similar/equivalent x86 processors.
2022-04-12 11:36 PM
Well check the STM32G4 which has cordic and Fmac, tainted for motor application. Due to cost to make a chip, float or double seems not always required.... in robotics
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.