2018-10-23 7:09 AM
For example timer A: is it low-speed (APB1) 'APB1 timer clock' or high-speed APB2 'APB2 timer clock'?
I read the timer and RCC sections but could not figure this out...
Can you tell me where this is documented?
Thanks!
Solved! Go to Solution.
2018-10-23 10:48 AM
PA, the nice clock diagram in CubeMX does not show which timers are on which clock, which was the original question. In the reference for the particular part I was looking at, the information was not in the RCC section nor the timer section, nor is there an "interconnection section". But it is in the datasheet, and in the overview block diagram. Thanks JW and Clive!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.