2022-06-14 8:15 AM
Hello,
I have an issue with my DAC. I am using a Nucleo STM32L476RG and my project consist of acquiring data from a mems microphone over i2S using the SAI and then send it to the DAC in order to view it with an oscilloscope.
First I initialize the DAC, SAI and a UART. During the while loop I acquire 6 words of 8 bits from the MEMS and use the first three in order to get my microphone value. I need to offset this data in order to put it in the range of the DAC and it worked too. The issue arrise when I try to divide the peak to peak amplitude by a factor of 10 for example. When not dividing I see my signal clear on the oscilloscope but when I try to divide the signal is unreadable .
So far, i have tried to cast as much as possible the type of my variables, change the DAC alignement but nothing works.
Help appreciated,
Sincerely
2022-06-14 9:38 AM
// Need data in left 12 bits of 32bit liData
if (HAL_DAC_SetValue(&hdac1, DAC_CHANNEL_1, DAC_ALIGN_12B_L, liData) != HAL_OK)
//This seems to create 24bit data? Is it signed or unsigned?
//Create an integer from the 3 words of the microphone
liData = tuiBuffer[0] << 8;
liData = (((liData | tuiBuffer[1]) << 8) | tuiBuffer[2]);
// Need data in 32bit values before shifting, else upper bits discarded during shift,
// and we want in top of 32bit:
lidata = ((uint32_t)tuiBuffer[0]) << 24 + ((uint32_t)tuiBuffer[1]) << 16 + ((uint32_t)tuiBuffer[0]) <<8;
//This looks like a shift to centre of 16bit(65536/2=32768), not 32bit, and not a divide
//I am trying to divide here
liData = 32765 + liData;
//Maybe
liData = liData + 0x7FFFFFFF; //Centre of 32bit
Paul
2022-06-14 9:52 AM
Use a PC with example data-sets to test/analyze algorithms
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.