2017-10-27 10:36 AM
What is Dual Address Mode in I2C Handle?
#i2c-addressing2017-10-28 12:47 AM
Hello!
Dual Address mode is valid only in slave mode.
Dual Address mode in I2c handle can have two values, I2C_DUALADDRESS_DISABLE or enabled
When enabled(ENDUAL bit of I2C_OAR2 register is set) . OwnAddress2 (in same handle) used also as valid slave address for device regognition by the Master of I2C Bus.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.