2024-01-26 5:59 AM
I'm developing a new project based on STM32G431RB using STM32CubeIDE 14.1.0 on macOS
I'm having touble where the program will hang at the first call of HAL_Delay() and digging deeper it's hanging because HAL_GetTick always returns 0
It looks like the SysTick timer is not running, or it's interrupt is not being called.
I do not have interrupts enabled on any other peripherals.
I have TIM1 configured as CH1_CH1N and that is working.
I have TIM2 configured in Encoder mode, and that is working too.
The only thing that is not working seems to be the System Timer.
What could I possibly have done to disable it?
My clock source is set to HSI
Here is my "main"
int main(void)
{
/* USER CODE BEGIN 1 */
uint8_t msg[64];
uint32_t lastCount;
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_ADC1_Init();
MX_TIM2_Init();
MX_USART2_UART_Init();
MX_SPI1_Init();
MX_TIM1_Init();
/* USER CODE BEGIN 2 */
HAL_TIM_Encoder_Start(&htim2, TIM_CHANNEL_ALL);
HAL_Delay(100); /* <-- IT HANGS HERE !!! */
brake_set();
lastCount = TIM2->CNT;
sprintf((char*) msg, "Startup count: %ld\r\n", lastCount);
HAL_UART_Transmit(&huart2, msg, strlen((char*) msg), 500);
motor_spinup_test();
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1) {
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
It hangs where I've shown in the comment above at HAL_Delay(100)
Any ideas?
Solved! Go to Solution.
2024-01-26 10:33 AM
The nucleo uses option bytes to boot into flash. Are yours set to do the same?
2024-01-26 10:37 AM
>>The nucleo uses option bytes to boot into flash. Are yours set to do the same?
Oooh now that sounds like something I should check. I'll check that now...
2024-01-26 10:41 AM
@TDK You're a genuis - thank you. I used STM32CubeProgrammer to set the option bytes and the problem has gone away.
Now if only there was a way to programme option bytes using the CuveIDE...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.