2020-01-13 3:07 PM
which one is more advantageous to work with as a Student and developer.
2020-01-16 7:38 AM
Hello @RSham.1 ,
The choice it depends on your needs and on application requirements.
I will recommend to review the STM32F401RE and STM32F446RE Overviews and compare the key features.
Best Regards,
Imen
2020-01-16 8:00 AM
The F446RE is a more powerful part.
Consider also using NUCLEO-144 boards, there is better pin escape, and VCP support.
2020-01-21 1:05 PM
U mean i terms of clock frequency or any thing else too?
2020-01-21 1:08 PM
I tried but couldn't notic rmuch other than in clock frequency .
2020-01-21 1:41 PM
The specs were pointed too above
401RE 84 MHZ FLASH:512KB RAM:96KB, TIM:11, U(S)ART:3 ADC:1, DAC:0, CAN:0
446RE 180 MHZ FLASH:512KB RAM:128KB, TIM:17, U(S)ART:6, ADC:3, DAC:2, CAN:2
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.