2017-09-13 10:06 AM
Hi all,
I am using a STM32f103C8T6 (blue pill), one of these $2 ebay boards, and I am having a really hard time getting some sort of dev environment set up with it.
I seem to have finally be able to get it to consistently program by setting the boot0 jumper to 1 and the boot1 jumper to 0, building my code in system workbench then flashing through the command like using stlink. So as it stand the board is not totally useless but I have no be able to get any debugging working. The closes I have to getting debugging working is to run openocd from the command line then I can run the debugger in system workbench. It successfully breaks at main but after 2 steps it given 'Error: JTAG failure -4' error through the opeocd terminal and system workbench debugger just hangs. I don't really have much experience with command line debugging and would really like to be able to debug in system workbench.
Does anyone have any idea's how to solve this issue or had any success with this board?On a side note, I do not have any problems with any of my otherboard with onboard debuggers so I don't think it is an issue with my system. More so the configuring for this board.
Cheers#stm32f103cbt6 #openocd2017-09-13 1:48 PM
External ST-LINK?
Connected what pins to what? SWDIO, SWCLK, NRST, GND, VCC?
Please provide a link to the specific board, with a schematic
2017-09-20 4:47 PM
Sorry if unclear, external ST-link meaning a st-link programmer (
http://www.st.com/en/development-tools/st-link-v2.html
) as the board does not have an on-board debugger.The board is the following:
http://wiki.stm32duino.com/index.php?title=Blue_Pill
and the pinout I used wasst-link board
RST -> NRSTSWDIO -> SWDIOGND -> GNDSWCLK-> SWCLK3.3V -> 3.3vCheers
2017-09-20 5:24 PM
People tend to hack up DISCO and NUCLEO boards to escape SWD connectivity. Pin 1 of the external version need power to connect via on-board buffers.
VTarget is an input, not a provider of power. Would need powering via 5V on micro-USB
What do ST-LINK Utilities report?
2017-11-13 4:52 AM
Check this thread
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.